MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
The MATLAB version being used is likely to be the main cause of the problem, rather than the method by which librealsense was installed. An official feature request was submitted to Intel in Janua...
-
There is not much documentation for software_device outside of the link above. My understanding of it is that instead of attaching a physical device such as a webcam, you provide the scripting wi...
-
Hi Rlt1 There was a case involving Error using librealsense_mex Frame didn't arrive within 15000 with the depth_example.m example program in January 2021. It was thought that the likely cause wa...
-
i installed the F200 camera and the R2 SDK on a Lenovo ThinkPad laptop. The installation was successful and the Camera Explorer and sample programs were able to work. I then tested whether it may ...
-
Hi Alessio Stella The official 1 meter cable supplied with the camera is validated by Intel for use with RealSense. You can extend the range with your own choice of cable but need to use a high q...
-
The R2 SDK expects an Intel Core processor that is 4th generation or newer. Your Lenovo has an 8th generation Intel Core, so a processor incompatibility is not likely to be the cause of the proble...
-
I recall a similar case in recent months where an F200 camera could not be detected in the Camera Explorer test application but worked with the R2 SDK's example programs. This may be because the R...
-
Hi Yonatan Sy As a starting point in investigating your case, could you use the instructions in the link below please to check if the camera has permission enabled to be accessed by applications i...
-
I do not have any librealsense-related LXD references to check. There was a past Docker case though where a RealSense user got it working by ensuring that the host and container kernel versions ma...
-
Which computer / computing device are you using please? Is it a PC, or a developer board such as Nvidia Jetson?