MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Bbiehler It has been stated in a past case by the Chief Technical Officer of the RealSense Group at Intel (agrunnet) that for an object to be reliably trackable, it should have at least 9 pixel...
-
Please do update about your case here after having a look. Thanks!
-
The semi-random dot pattern emitted by the built-in projector of the camera will not negatively affect the cameras when FOVs are overlapped. In fact, it can be beneficial to have an increased numb...
-
Hi Alessio Stella Structured Light is used by the RealSense SR300 and SR305 camera models. Multiple SR300 / SR305 cameras can interfere with each other. The 400 Series cameras use a different dep...
-
That is correct, external projectors can provide greater projection range due to higher power. This is demonstrated by the image below from a past RealSense case of an external LED projector used ...
-
Hi Saad Azhar 1 and 2. RGB is not required for generating a RealSense depth image (which is produced by the infrared sensors), though it can be useful for aligning depth to color. On the D435 / ...
-
A USB device may heat up rapidly if there is a fault in the USB cable or in the USB port. There was also once a case of a developer board overheating, with accompanying camera ASIC and Projector ...
-
And there is no difference if you unplug the micro end of the cable from the side of the camera, turn it upside down and re-insert it into the camera (as USB-C cables are two-way insertion on their...
-
Hi O Patrouix Do you hear the USB insertion sound effect of Windows (doo-doo-doo-doo) when inserting the camera with the problem into a USB port on your hub, please? If not, is there any reaction ...
-
If you have questions about the L515 model or the L515's Dimensional Weight Software then please create a new case on this forum so that RealSense specialists in those subjects can assist you. In r...