MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Zhouyangjunjian In your rs-pcl-color.cpp script, have you modified line 169 (which defines the color stream)? It should use RGB8 format by default. But if the line had been modified to set th...
-
Hi Yenyen841009 The D457 model can operate in USB mode by moving a switch in the casing. However, if you do not need a GMSL/FAKRA connection then D456 has the same water-resistant casing as th...
-
Hi Tvasco90 As your project does not flicker when using the D415 camera model but does with a D455f, I would first recommend setting the D455f's IR emitter to Always On. The D415's projector comp...
-
Hi Dsyuan Are you able to access the RealSense Viewer tool? If you are, please try resetting the camera to its factory-new default calibration using the instructions at the link below. https://gi...
-
I compared the above list of parameters to the values for those parameters in the selection of downloadable json files on the Visual Presets page. In most cases the only parameters that were diffe...
-
Hello, are you asking about checking functions in a script with Intellisense to perform actions such as code completion, please? If you are using Intellisense then the known issue of problems w...
-
In regard to checking whether the preset has been applied successfully, this could not be done when importing a json file, unless you query the value of one of the settings in the json file (such a...
-
Hi Clement Foreau The in-built Visual Presets are not able to be defined in a json, unfortunately. Visual Presets are another name for json files, so a json cannot be set within another json. An ...
-
Hi Seungsoo Lee In a discussion at the link below, I suggest fixing the /video addresses using symbolic links with the udev device handling rules. https://github.com/IntelRealSense/librealsense/is...
-
The D456 and D457 models have an IP65 rated casing that protects against entry into the camera by dust or by water jets from any direction, making them a good choice for outdoor applications. Fo...