D456 vs D455f
Hi all, I'm confused in choosing D456 or D455f. I wonder how better if i buy D455f, which with IR pass filter, rather D456? In my case, usually, inside and static, waterproof function is not require.
BTW, I will not consider D457, cause i wanna connect with the usb-c.
-
Hi Yenyen841009
The D457 model can operate in USB mode by moving a switch in the casing. However, if you do not need a GMSL/FAKRA connection then D456 has the same water-resistant casing as the D457.
The light-blocking filter on D455f can provide an improved depth image by being able to better deal with light reflections and negate disruptive 'repetitive patterns' (repeating horizontal or vertical patterns in the scene such as tiles on the ceiling or floor). So if you do not require waterproofing then D455f is likely to be the appropriate choice for you.
Please sign in to leave a comment.
Comments
1 comment