MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
In a past case I tested a D435i with a similar thin and long object, a toothpick. https://github.com/IntelRealSense/librealsense/issues/8228
-
Also, if you would prefer a small form-factor that lends itself to portability but need desktop power, an Intel NUC may suit you. It is available in a wide range of price-points and configurations...
-
Hi Aljosa Any of the listed i7 Intel Core CPUs that are modern 11th Generation (indicated by the '11' in their CPU model code) should be sufficient. An i5 should be able to handle two cameras simu...
-
1. RealSense cameras are a Class 1 laser device that is not harmful to human health, including the eyes, face and pregnancy. The RealSense range has extensive safety certification that can be fou...
-
Hi Payman Azari Creating 3D point cloud scans of small body parts such as nose, ears and mouth is achievable with a RealSense D435 or D435i camera model, though it requires some small adjustment o...
-
Creating a single application that can save each camera to an individual drive path would be slightly more complicated than saving all cameras to the same path. I would speculate that you could se...
-
Hi P Woronow Yes, RealSense 400 Series cameras including the D455 are compatible with Jetson Nano and the rest of the Jetson range of boards. They have separate installation instructions though. ...
-
Hi Asagllam In regard to choosing a ROS branch, the most recent versions supported by the RealSense ROS wrapper at the time of writing this are Noetic for ROS and Foxy for ROS2. The RealSense ca...
-
Hi Siukey It s possible for RealSense cameras to use light in visible or near-infrared (ranging from ~400-1000nm, with 850nm being a recommended frequency. More information about the infrared capa...
-
Hi A5020877 I hope that the link below about a similar Python case where the depth colours were reversed will be helpful to you. https://github.com/IntelRealSense/librealsense/issues/6856 Resource...