MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
You are very welcome. I am happy that we were able to help. :)
-
Thank you very much for the information. Does the image improve if you turn off the IR Emitter in the RealSense Viewer side-panel? You can turn it off by left-clicking on the blue box next to 'Em...
-
As you have not had a response yet from a support agent, I have referred your message by email to a senior member of Intel Support.
-
When the image looks this broken, the first action that I would usually recommend trying is to re-calibrate the camera. This can be done with the Custom Calibrator tool for the 400 Series cameras,...
-
I would recommend aligning to depth. Page 38 and 39 of the RealSense 400 Series custom calibration white paper document have information about writing parameters to a .txt file using the CustomRW t...
-
There is a known issue with using D435 and T265 together, where the D435 can prevent the T265 from being properly started if the D435 is the first device to start up. Details of it can be found in...
-
I have never heard of a built-in RealSense camera causing conflicts with internal PC hardware. The F200 camera should be mostly dormant when it is not in use. It is more likely that your laptop h...
-
I could not find anything definitively useful on the memory location error, though there was the suggestion that it might occur if OpenNI2 is trying to call an image when the camera is not active (...
-
24 FPS support for film-makers has been a requested feature by RealSense users. As far as I know, it is not on the developer roadmap though. I believe the reason for this is that they try not to ...
-
The RGB sensor on all of the 400 Series cameras is a rolling shutter type. In regard to the left and right IR imagers, the D435 and D435i's IR imager has a global shutter. Intel's guide to gettin...