RealSense Support

t265 and d435 Failed to claim USB interface error

Comments

4 comments

  • MartyG

    There is a known issue with using D435 and T265 together, where the D435 can prevent the T265 from being properly started if the D435 is the first device to start up.  Details of it can be found in the link below, which suggests a method to delay the D435's launch in ROS using code.

    https://github.com/IntelRealSense/realsense-ros/issues/774 

    0
    Comment actions Permalink
  • Erdynieve

    thanks for quick reply. I'll check it out

    0
    Comment actions Permalink
  • Kartikprakash3775

    I am facing the same issue when I try to run two t265 together. I am using the following launch method

    roslaunch realsense2_camera rs_camera.launch camera:=cam_1 serial_no:=845412111129 (in one terminal)

    roslaunch realsense2_camera rs_camera.launch camera:=cam_2 serial_no:=943222110577 (in another terminal)

    No matter how much delay is there in the two launches I keep getting the LIBSUB_ERROR_BUSY and other error messages similar to the post above.

    I will be so thankful if anyone can help me sort out this issue. Thanks!

    0
    Comment actions Permalink
  • MartyG

    I found an entry in the ROS wrapper documentation that states that launching multiple T265 in the wrapper is not currently supported.

    https://github.com/IntelRealSense/realsense-ros#work-with-multiple-cameras 

    The subject of using multiple T265 together via Librealsense instead of ROS is discussed in the link below by an Intel RealSense team representative.

    https://github.com/IntelRealSense/librealsense/issues/4961#issuecomment-537351418 

    0
    Comment actions Permalink

Please sign in to leave a comment.