MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Alkismichael1 Built-in RealSense cameras are significantly more difficult to fix than external USB RealSense cameras once a problem occurs with them. The place to turn to for support for such ...
-
Hi Smiddominikcz The link below leads to a video of an Intel seminar about using RealSense cameras to train a dataset for tracking body points. You can skip to the 16 minute stage in the video fo...
-
Hi 8care RealSense 400 Series cameras can run indefinitely so long as they remain within recommended temperature tolerances. They also incorporate a laser safety mechanism that will halve the las...
-
Hello Weiyiadas Could you provide more details please of the information that you are seeking? If you are planning to use four RealSense cameras for a multiple camera surround view on a vehicle t...
-
Hi Waddelat. I tested 300 FPS 848x100 mode recently in the RealSense Viewer program with D435i and D455. 300 FPS was streamable on the D435i but the maximum available selectable FPS on D455 for th...
-
Hi Jxpenggf I hope that the links below will be helpful in answering your question. https://github.com/IntelRealSense/librealsense/issues/7568 https://github.com/IntelRealSense/librealsense/issues...
-
A script with a simpler approach that does not use aligned frames is here: https://github.com/IntelRealSense/librealsense/issues/2832#issuecomment-443823647
-
Hi Anadig The link below describes a means to use export_to_ply to export colorized depth instead of the color frame. In that particular case though, the RealSense user apparently did not see a n...
-
Hi Michaelszeng I hope that the link below will be helpful to you. https://github.com/IntelRealSense/librealsense/issues/4796
-
Hi Jgladfelter The official Intel RealSense website states that the D455's error is less than 2% at 4 meters. The D455 has 2x the depth accuracy over distance of the D435. So at 6 meters distanc...