RealSense Support

Does the mipi camera access driver of AAEON® UP Squared Board support?

Comments

1 comment

  • MartyG

    Hello Weiyiadas  Could you provide more details please of the information that you are seeking? 

    If you are planning to use four RealSense cameras for a multiple camera surround view on a vehicle then that can certainly be achieved.

    If you would like to stream four cameras simultaneously with RealSense then an Nvidia board such as Nvidia Jetson would be a suitable computing device for multiple cameras attached to the same board, and the automotive industry is well supported by Nvidia with platforms such as DRIVE AGX.

    https://www.nvidia.com/en-us/self-driving-cars/

    The RealSense SDK software, if installed on the computing board, could also control the four cameras and their visual streams.  So using drivers for the nvp6324, max9286 or ds90ub964 may be unnecessary if you are hoping to connect multiple RealSense cameras to the same board, as the RealSense SDK software already supports that.

    0
    Comment actions Permalink

Please sign in to leave a comment.