RealSense Support

RealSense™ Depth Camera D455 Depth Accuracy?

Comments

1 comment

  • MartyG

    Hi Jgladfelter  The official Intel RealSense website states that the D455's error is less than 2% at 4 meters. 

    The D455 has 2x the depth accuracy over distance of the D435.  So at 6 meters distance, the D455 has the same depth accuracy as the D435 has at 3 meters

    0
    Comment actions Permalink

Please sign in to leave a comment.