MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Stevenkruyswijk If your Mac is using MacOS Monterey then there are a couple of methods that you could use to install the librealsense SDK on your Mac. Both methods work for x64 and Apple Silic...
-
Hi Gururaja K As you mention, the minimum power draw will be around 5 V. In regard to maximum power draw, it is recommendable to budget for 2W per camera. Yes, disconnection is likely to oc...
-
You are very welcome. I'm pleased to hear that your needs were met by the camera. Thanks so much for the detailed update!
-
Hi David Workacc08 The VF0800 was also known as the RealSense F200. It is not supported by modern RealSense software but there was a programming SDK for Ubuntu that supported it and is still avai...
-
Yes. Not every setting in the Viewer is exported to a json file, but param-secondpeakdelta should be included in the file by the export. That file can then be loaded into the program and the sett...
-
It can be set in a custom json camera configuration file (also known as a Visual Preset) by configuring the parameter below: param-secondpeakdelta https://github.com/IntelRealSense/librealsense/is...
-
If the camera is moved close to an object then the depth image will start to break up below a certain distance from the object, as RealSense cameras have a minimum depth sensing distance. If t...
-
Hi Edenclaire8 The RealSense SDK's pyrealsense2 example program opencv_pointcloud_viewer.py has controls for rotating a pointcloud by dragging it around with the left mouse button, plus some addit...
-
If Open3D is not a compulsory requirement of your project then you could explore using the free open-source 3D tool MeshLab to import your ply, convert it to a mesh and edit it. A guide for doing ...
-
Hi Conor Mckenna The D405 camera model is not equipped with an infrared dot pattern projector component like other models in the RealSense 400 Series are, so smooth plain surfaces can be difficult...