Karthikeyan Yuvraj
- Total activity 19
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 4
Posts
Recent activity by Karthikeyan Yuvraj-
Bayer filter applied on IR image from D455
Hello All,D455 (at firmware: 05.13.00.50) image below is from the IR sensors (configured at 1280x800 resolution and IR images are at Y16 format).As you see the image below has the bayer filter appl...
-
IR Image with auto ir exposure is dimmer than manual on D415 cameras
This is an IR image (of IR1 and IR2) with auto-exposure enabled: and this is an IR image (of IR1 and IR2) with manual exposure: Any thoughts on why the IR image with auto-exposure enabled is dimme...
-
Capturing images from a D415 and D455 simultaneously.
Hello All,I am streaming the depth and RGB images from a scene simultaneously using D415 and a D455 camera. Will this cause interference in the depth images between the 2 cameras?. Let me know. Tha...
-
Dynamic Calibration tool intrinsics
Hello All, I am using the D400 series dynamic calibration tool. I see this tool provides an option to read and write calibration directly to/from the camera. If I need to write intrinsics to RGB, ...