Camporeale Andrea

  • Total activity 9
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 4

Activity overview

Latest activity by Camporeale Andrea
  • Camporeale Andrea created a post,

    D455 RGB sensor confirmation

    Hi All, I would like to get confirmed what RGB sesnor is mounted in D455 depth camera. The latest datasheet I can find is V10, dated February 2021, that I can dowload from: https://dev.intelrealsen...

  • Camporeale Andrea created a post,

    Camera connection and disconnection / C#

    Hi All, am monitoring the connection/disconnection ot 2 D455 cameras. Below is the code and the result I get when I connect the two cameras and the disconect one of them. When a camera is disconnec...

  • Camporeale Andrea commented,

    Hello MartyG, many thanks for your fast reply! rgrds Andrea  

  • Camporeale Andrea created a post,

    D455 default stream porfile

    Hi All, on D455, updated with latest FW, when I read the StreamProfiles from the MotionModule I get that 2 streams have the ".IsDefault" attribyte set to true - please see the dump below. The 2 oth...

  • Camporeale Andrea created a post,

    D455 auxiliary connector - mechanical issue?

    Hi All, I am working on a multi-camera setup with Realsense D455. I wanted to HW-synch the devices by using their 9 pin auxiliary connector. I think that I have ordered the appropriate connector bo...