RealSense Support

[D435i] Improve RGB sensor performance for moving objects detection on a conveyor

Comments

4 comments

  • MartyG

    Hi Fpelegri  You could reduce RGB blurring on the D435i model by using one of the following methods:

     

    1.  If you have auto-exposure enabled, set depth FPS to 30 and RGB FPS to 60.  This should compensate for the slower speed of the RGB sensor's 'rolling' shutter compared to the faster 'global' shutter on the depth sensor.  

     

    2.  Disable RGB auto-exposure, set RGB FPS to '6' (not 60) and set a manual RGB exposure of around '70'.

     

    Alternatively, if you are able to change to a different RealSense model then the D455 has a fast global shutter on both the RGB and depth sensors.

    0
    Comment actions Permalink
  • Fpelegri

    Hi MartyG!

    Thanks for the fast feedback. Second option you mentioned already helped to understand that lower FPS could increase brightness and blur-less to the frame, but due to fast moving object and the camera's rolling shutter mode, the object could show deformed and that could cause another issue.

    One of my concerns was the brightness received on the sensor due to low exposure, is there any other recommended parameter option to adjust (I use GAIN).

    I am considering the option to get D455 camera for my solution, I think its RGB sensor could get more bright and static frames due to its properties (larger sensor pixel size and global shutter). Could I have a sample frame of the D455 with a moving object with/without a barcode? Also if possible compared to d435i.

     

    0
    Comment actions Permalink
  • MartyG

    You could try disabling the RGB option Auto White Balance so that a manual value is used for white balance.

     

    A barcode will be sharper if the RGB Sharpness option is maximized to '100'

     

    Below are images captured during fast camera motion with and without a barcode for D435i and D455.  They were taken with FPS of 6 for D435i and 5 for D455 (as D455's minimum FPs is 5 instead of 6), and manual RGB exposure set to 78 and gain maximized to 128.

     

    D455 was noticeably brighter and also did not have distortion (demonstrated by the bendy bottle on D435i).

     

    D435i

     

     

    D455

     

     

     

    0
    Comment actions Permalink
  • Fpelegri

    Really clarifying thanks! I'll test those recommended parameter values and share results.

    Regarding camera, D455 has an obvious improved frame result.

    Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.