RealSense Support

D435 vs D405 IR lens comparison

Comments

4 comments

  • MartyX Grover

    Hi Henry, the D401 / D405 have hardware differences to the other 400 Series stereo depth camera models that make them capable of sub-millimeter accurate, high quality images at very close range. 

    RGB is obtained from the depth sensor instead of having a separate RGB sensor and then the Image Signal Processor (ISP) on the new Vision Processor D4 Board V4 enhances the RGB.

    The D401 / D405 are not equipped with a built-in infrared projector.  The left and right imagers are equipped with IR Cut filters that exclude infrared frequencies from being visible to the camera.  The D401 / D405 therefore cannot see infrared patterns produced by external IR pattern projectors or the built-in projectors of other 400 Series camera models that are equipped with one. 

    Having a short stereo baseline (the distance between the center of the left and right imagers) can also help to avoid blurring at very close range that would occur on a D435 if placed at extreme close distance from a surface.

    0
    Comment actions Permalink
  • Henry

    I'm testing the D435 IR camera at distances around 250mm away and it's still quite blurry.  Is the raw unrectified IR stream available?

    0
    Comment actions Permalink
  • MartyX Grover

    The Y16 infrared stream is unrectified because it is used for camera calibration.  It has a smaller number of supported resolution and FPS modes than Y8 though.

    0
    Comment actions Permalink
  • Info

    Hello Henry, D435 minimum working distance is around 500mm

    0
    Comment actions Permalink

Please sign in to leave a comment.