Henry

  • Total activity 11
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 4

Activity overview

Latest activity by Henry
  • Henry created a post,

    D401 module questions

    I have used the D405 camera and have some questions on switching to the D401. 1) If I buy the D401 camera module and the D4 vision board for the D401, is the calibration data stored on the D4 visio...

  • Henry commented,

    I'm testing the D435 IR camera at distances around 250mm away and it's still quite blurry.  Is the raw unrectified IR stream available?

  • Henry created a post,

    D435 vs D405 IR lens comparison

    I'm trying to understand performance of the images produced by the D405/D401 vs the D435.  The  raw D405 IR image seems much sharper than the D435 which I can say is blurry.  Is this due to it bein...

  • Henry commented,

    Thanks yes I do have a D435 - sorry for the error.  Increasing sharpness does seem to help so I will use that but the D405 seems to focus a lot closer so may be a better solution though without a d...

  • Henry created a post,

    D405 Focus and Depth of Field vs D430?

    What are the lengths that the D405 RGB camera can resolve clearly vs the D430?  I have a D430 and lengths of around 120mm it appears pretty blurry in the RGB but still usable though not ideal.  Eg ...

  • Henry commented,

    As far reference:  Intrinsic of "Color" / 1920x1080 / {YUYV/RGB8/BGR8/RGBA8/BGRA8/Y16/RAW16}  Width:        1920  Height:       1080  PPX:          974.587890625  PPY:          558.511108398438  Fx...

  • Henry created a post,

    Confusion about Camera Extrinsics and how to use

    I want to utilize the Color camera and make some coordinate transforms using AprilTags for depth to compare against the Intel camera distance measurements. 1) I grab an color and a depth image.  I ...