D415 Quit Working
So i bought this D415 from amazon in september 2021, ive used it once or twice after i got it to test if it worked and to check it out, and i was happy with the performace. This week i finally got around to integrating it into my project, and when i hooked it up, i get nothing. the OS doesnt see it, i re-installed the SDK, tried it on multiple machines, *where it worked before* and i get no response at all from the camera.. any suggestions?
-
Hi Orflyfisher82 Which OS are you using the camera with, please?
-
You know i think it was 20.04 -
This is current : Linux ThinkPad-T510 5.13.0-30-generic #33~20.04.1-Ubuntu SMP Mon Feb 7 14:25:10 UTC 2022 x86_64 x86_64 x86_64 GNU/Linux
I thought when you compiled the sdk from source it built the modules for your kernel -i used the apt repo to install librealsense2, when it didnt work i uninstalled and built from source via sdk_source_dir/scripts/patch-uvcvideo-ubuntu-mainline.sh
it compiled and installed correctly.. -
When building from source, the most recent configuration supported in SDK version 2.50.0 at the time of writing this is Ubuntu 20.04 and kernel 5.11. The SDK is able to work with newer kernels but there may be unpredictable consequences in regards to stability and there have been problems reported with using kernel 5.13.
The most stable 5.11 kernel has been reported recently by RealSense users to be 5.11.0-34-generic.
If you continue to experience kernel related conflicts then there is the option of building librealsense from source code with the RSUSB backend method, which is not dependent on Linux versions or kernel versions and does not require patching.
When building from packages, the most recent supported kernel listed is 5.4
More information about all of the above information can be found at the link below.
https://github.com/IntelRealSense/librealsense/issues/10288#issuecomment-1059101026
-
right, i just figured that out right before you posted this, and was trying to figure out how far into 5.11 i could go. i was going to try 5.11.0-44 but ill drop back further. thanks for the info. if i cant get a response from the camera after i switch kernels ill post back here. thanks for the help buddy.
Please sign in to leave a comment.
Comments
6 comments