View my account

About make sure FOV specification of D435i

Comments

1 comment

  • MartyX Grover

    Hi Getomboy  Thanks very much for your questions.

     

    1.  Pages 66-68 of the current edition of the data sheet document for the 400 Series cameras describe FOV.  The paper states that "The depth field of view is the common overlap of the individual left and right Imager field of view for which Vision Processor D4 provides depth data".

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

     

     

    2.  For 400 Series camera models that have a casing, depth measurement begins at the front glass instead of the camera lenses.  You can find the ground truth of measurements by adding a minus-value to measurements, as described at the bottom of page 73 of the current data sheet edition.  As suggested by your kindly provided diagrams, on the D435 and D435i models you should add -4.2 mm to the depth measurements to find the ground truth.

     

    3.  The origin point of the coordinate system of the 400 Series cameras is the center of the left infrared imager.  The left IR imager is on the right side of the camera when viewing it from the front like in the mechanical drawing that you provided.

    0
    Comment actions Permalink

Please sign in to leave a comment.