Getomboy

  • Total activity 16
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 6

Activity overview

Latest activity by Getomboy
  • Getomboy created a post,

    About make sure FOV specification of D435i

    Hi, Nearly, we need to redesign the application of D435i. So we need to critical make sure FOV specification. Currently, using the resolution of 424*240 that approach FOV HD size.  I've three quest...

  • Getomboy created a post,

    About FoV issue of D435i

    Hi, Recently, I use D435i to catch the point cloud data that have the unstable condition of FoV.  The unstable condition is sometimes following FoV specification, but sometimes bigger than FoV spec...

  • Getomboy commented,

    Hi MartyG, I've used your solution that the camera has done resetting device. Unfortunately,  the error still exist. Could you have another suggestion? Or I need to check something? Thanks.

  • Getomboy commented,

    Excuse me. Could you have the specific approach? Such as SOP of the resetting parameter. I cannot catch your solution. Or the machine is broken ? Thanks again.

  • Getomboy created a post,

    About the camera connection issue on ROS

    Hi Intel Support, I've a problem that about D435i load the log files to connect PC on ROS. I use the launch file to test the camera connection from the below address. (rs_camera.launch) git clone b...

  • Getomboy created a post,

    How to synchronous control multi-camera without using series number?

    Hi Realsense supporter, Currently I use the series number to control dual D435i cam. However, the device do mass production that cannot use the series number method. Because We cannot check every c...

  • Getomboy commented,

    Hi MartyG thanks for your reply. I still having trouble on filtering the flying pixel like the picture below,  

  • Getomboy created a post,

    How to filter the noise of D435i that the spotlight making ?

    Dear Intel Service, When my camera turn the specific angle, the spotlight makes the camera noise (like flying pixel) to let my function failure. However, I cannot change the camera angle, it is our...

  • Getomboy created a post,

    How to filter the (flying pixel) noise of D435i?

    Hi, I'm using D435i camera on my AGV. Under the normal condition that FoV of camera is without occlusion, it has no noise on AGV working. (Shown as the below) When AGV with the shelf, FoV of camer...