RealSense Support

Realsense D435i not giving RGB data. realsense-viewer is showing D430

Comments

11 comments

  • Official comment
    Rizvi, Sahira

    Hi Kaustubh Joshi1997,

    Based on your description of the issue, your D435i​ is faulty and should be returned or exchanged.

    • If you did not purchase the unit from the Intel Store, contact your distributor for a return.

    We apologize for the inconvenience this has caused.

    Sincerely,

    Sahira Rizvi

     

    Comment actions Permalink
  • MartyG

    Hi Kaustubh Joshi1997  Has the camera been detectable in the Viewer as a D435i before today, or has it been D430i from the first time that you used the camera please?

    Does going to the More option at the top of the Viewer's side-panel and selecting the Hardware Reset option from its drop-down menu to reset the camera make a difference to the camera name that is displayed?

    0
    Comment actions Permalink
  • Kaustubh Joshi1997

    Hi Marty,

    It is showing D430i since the beginning and I am not getting any RGB stream.

    I tried your suggestion but it is not making any difference.

    Kindly let me know what else can be  done. Thank you.

    0
    Comment actions Permalink
  • MartyX Grover

    What computer are you using with the camera please (PC, Mac, etc) and which operating system (Windows, Ubuntu, MacOS, etc)

    0
    Comment actions Permalink
  • Kaustubh Joshi1997

    I have tried it on Windows as well as Ubuntu 18.04

    0
    Comment actions Permalink
  • MartyX Grover

    Thank you very much.  Next, could you try the rs-capture RealSense example program to see whether the RGB image is displayed please.  Doing so will provide information about whether or not the problem is limited to the RealSense Viewer tool only.

    The link below has instructions for launching the rs-capture example in Windows.

    https://github.com/IntelRealSense/librealsense/issues/8024#issuecomment-747630656

    0
    Comment actions Permalink
  • Kaustubh Joshi1997

    Thanks a lot. I will check it and let you know

    0
    Comment actions Permalink
  • Kaustubh Joshi1997

    Hi Marty. I am not getting the RGB stream when I follow the steps above. I am still getting the stereo output.
    Kindly let me know what can be done. Thank you.

    0
    Comment actions Permalink
  • MartyX Grover

    Thanks very much for testing with the rs-camera example.

    Next, let's test whether the camera is capable of accessing the RGB outside of the RealSense SDK by using the built-in Camera app of Windows that can be used to test ordinary webcams.  Please input the term camera into the text box at the bottom of your Windows screen, next to the corner button where you shut down the PC.  

     

    If you initially have a blank black window in the app, left-click on the topmost icon highlighted with an arrow in the image below to toggle the view to the D435i.  If the message Can't start your camera appears then just click the Close button to skip past it.

    Does the RGB display in the Camera app on your Windows computer?

     

    0
    Comment actions Permalink
  • Kaustubh Joshi1997

    I am getting the following error:

    “Can’t start your camera”
    “If you’re sure that the camera is connected and installed properly, try checking for updated drivers”

    Error code: 0xA00F4262 (0xC00D5212)

    The only option I am able to see are b “Learn More” and “Okay”

    0
    Comment actions Permalink
  • MartyX Grover

    I will refer your case to a team member of the Intel RealSense Customer Support forum for further advice.

    Hi @...  This is a case of a D435i camera that is enumerated as a D430i (a rare error indicating that the RGB sensor is not being detected by the firmware driver).  The RGB was not accessible in RealSense SDK applications, nor outside of the SDK in the Windows built-in app Camera for RGB webcams.  Changing the firmware version made no difference.  

    A physical cause of this issue may be a disconnection of the D435i's RGB cable inside the camera casing.

    Could you provide advice to Kaustubh Joshi1997 please?  Thanks very much!

     

    0
    Comment actions Permalink

Please sign in to leave a comment.