RealSense Support

EXC_BAD_ACCESS On MacOS

Comments

16 comments

  • Official comment
    Jesus Garcia

    Hello David,

    The RealSense L515, as well as other RealSense cameras that have an IMU, do not fully function on Mac. We have found that RGB may work, but Depth and IMU streaming do not work. Our engineering team is looking further into this but there is no timeframe for a fix yet.

    This is caused by issue in Mac OS with libusb, its fairly wide-spread, affecting different HID devices (IMU, joysticks, etc..)
    See:
    https://github.com/libusb/libusb/issues/158
    https://github.com/pyusb/pyusb/issues/208
    https://pyusb-users.narkive.com/ZUDlHEA7/help-with-reading-data-from-hid-device
    https://stackoverflow.com/questions/20253350/unable-to-claim-usb-interface-with-c-libusb-on-mac-os-x

    Comment actions Permalink
  • Jesus Garcia

    Hello David,

    We are looking into your issue.

    Regards,

    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • David Thevenin

    Thanks 

    here more information related to the installation:

    macOS       10.57.7
    libusb          1.0.23
    pkg-config   0.29.2_3
    glfw             3.3.2

    Regards

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello David,

    We were able to reproduce your issue. In our case, RealSense Viewer crashed too. We will forward this issue to engineering so they can take a look at it.

    Regards,
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • David Thevenin

    Hi Jesus Garcia

    Do you have update on that issue?
    Because of this bug, I can't use the cameras on MacOS; it's blocking.

    In the time being I could down grade to a previous version of the SDK for instance...

    Regards

    David

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello David,

    I have not heard back from engineering regarding this issue.I am checking with them again.

    Regards,

    Jesus

    0
    Comment actions Permalink
  • David Thevenin

    Hi Jesus

    Thanks.

    If it can help, I could test the pull request on my Mac.

    Bests

    David

    0
    Comment actions Permalink
  • Jesus Garcia

    Hi David,

    We are still waiting to hear back from engineering.

    Regards,

    Jesus

    0
    Comment actions Permalink
  • David Thevenin

    Hi Jesus

    I understand; thanks for the investigation and the summary.

    I did test on a fresh installed macOS, means that 

    kextstat | grep -v apple

    return nothing, and it does not work too.

     

    Anyway, since my cameras do not work on Mac, at least for now, what is procedure to return them?

     

    Best regards

    David

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello David,

    • If you purchased your camera from the Intel RealSense Store, please sign in to your account on http://www.intelrealsense.com and go to My Account -> My Orders -> Return or Replace Items or open a ticket here.
    • If you did not purchase your Intel RealSense Camera from the Intel Store, contact your distributor for a return.
    0
    Comment actions Permalink
  • Jesus Garcia

    Hello David,

    Before you return the cameras, have you considered moving to a different platform such as a Windows or Linux host?

    Also, do you require the IMU capability of the L515 or do you just need depth and RGB?

    The IMU not working is a known issue but our engineers say depth is supposed to work. They are looking into the problem with depth on MacOS.

    Regards,

    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • David Thevenin

    Hi Jesus

    I do not have PC, only Macs.

    I do consider Linux into a Virtual Machine, but it looks to me a bit complicated. I'm evaluating the solution tho.

    But for now I'm still considering to return them, since the camera are not working on Mac.

    Regards

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello David,

    Thank you for your explanation.

    Unfortunately, a Linux VM on your MacOS will not solve your problem. RealSense cameras do not work well in virtual environments, much less when the host operating system is not fully supported.

    Do you require IMU capabilities?

    Regards,

    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Intel

    We too was looking forward to developing for the Mac. D455 just arrived. 
    Ps. I'm not Intel, as the name suggests. Might be taking the first part of the email i've used intel@emers..

    0
    Comment actions Permalink
  • Philip Broser

    Hi Garcia,

    I ran into the same problem and while searching I found this thread.

    I am using an Mac Book Pro with 11.4 and a L515 attached with USB 3.

    The connection between the camera and realsense library is unstable. 

    The

    hello-realsense 

    tool either says it cannot find the camer or not claim the USB 7 port.

    After reeboting the system the camera works for a while and then suddenly crashes. 

    With the above result. Have you found a solution to the connection problem?

    Greetings

    Philip

     

    0
    Comment actions Permalink
  • Philip Broser

    Thats part of the crash log from

    ./rs-capture  .

    The tool did run for a while with 

    RGB, depth and infrared plus gyroscoeope

    but when it started it showed:

    Philips-MBP:capture philipbroser$ ./rs-capture 

     26/07 23:03:20,455 ERROR [0x1130d6e00] (handle-libusb.h:95) failed to claim usb interface: 7, error: RS2_USB_STATUS_ACCESS

     26/07 23:03:20,456 ERROR [0x1130d6e00] (handle-libusb.h:95) failed to claim usb interface: 7, error: RS2_USB_STATUS_ACCESS

     

     it ran for about 20 seconds and then crashed: 

     

    Process:               rs-capture [5032]
    Path:                  /Users/USER/Documents/*/rs-capture
    Identifier:            rs-capture
    Version:               0
    Code Type:             X86-64 (Native)
    Parent Process:        bash [1099]
    Responsible:           Terminal [546]
    User ID:               501
     
    Date/Time:             2021-07-26 23:04:08.296 +0200
    OS Version:            macOS 11.4 (20F71)
    Report Version:        12
    Bridge OS Version:     5.4 (18P4663)
    Anonymous UUID:        9ECADC66-5F87-D26B-C9B3-8082EDE18AC3
     
     
    Time Awake Since Boot: 2700 seconds
     
    System Integrity Protection: enabled
     
    Crashed Thread:        35
     
    Exception Type:        EXC_BAD_ACCESS (SIGSEGV)
    Exception Codes:       KERN_INVALID_ADDRESS at 0x0000000000000000
    Exception Note:        EXC_CORPSE_NOTIFY
     
    Termination Signal:    Segmentation fault: 11
    Termination Reason:    Namespace SIGNAL, Code 0xb
    Terminating Process:   exc handler [5032]
     
    VM Regions Near 0:
    --> 
        __TEXT                      109c4e000-109cc6000    [  480K] r-x/r-x SM=COW  /Users/*/Documents/*
     
    Thread 0:: Dispatch queue: com.apple.main-thread
    0   libsystem_kernel.dylib         0x00007fff2035ecde __psynch_cvwait + 10
    1   libsystem_pthread.dylib       0x00007fff20391e49 _pthread_cond_wait + 1298
    2   libc++.1.dylib                 0x00007fff202fae03 std::__1::condition_variable::__do_timed_wait(std::__1::unique_lock<std::__1::mutex>&, std::__1::chrono::time_point<std::__1::chrono::system_clock, std::__1::chrono::duration<long long, std::__1::ratio<1l, 1000000000l> > >) + 93
    3   librealsense2.2.48.0.dylib     0x0000000109f8d9e6 std::__1::cv_status std::__1::condition_variable::wait_for<long long, std::__1::ratio<1l, 1000000000l> >(std::__1::unique_lock<std::__1::mutex>&, std::__1::chrono::duration<long long, std::__1::ratio<1l, 1000000000l> > const&) + 358 (__mutex_base:468)
    4   librealsense2.2.48.0.dylib     0x0000000109f8d70c void std::__1::condition_variable::__do_timed_wait<std::__1::chrono::steady_clock>(std::__1::unique_lock<std::__1::mutex>&, std::__1::chrono::time_point<std::__1::chrono::steady_clock, std::__1::chrono::duration<long long, std::__1::ratio<1l, 1000000000l> > >) + 92 (__mutex_base:523)
    5   librealsense2.2.48.0.dylib     0x0000000109f8d4ab std::__1::cv_status std::__1::condition_variable::wait_until<std::__1::chrono::steady_clock, std::__1::chrono::duration<long long, std::__1::ratio<1l, 1000000000l> > >(std::__1::unique_lock<std::__1::mutex>&, std::__1::chrono::time_point<std::__1::chrono::steady_clock, std::__1::chrono::duration<long long, std::__1::ratio<1l, 1000000000l> > > const&) + 139 (__mutex_base:426)
    6   librealsense2.2.48.0.dylib     0x000000010aaf1c29 _ZNSt3__118condition_variable10wait_untilINS_6chrono12steady_clockENS2_8durationIxNS_5ratioILl1ELl1000000000EEEEEZN21single_consumer_queueIN12librealsense12frame_holderEE7dequeueEPSA_jEUlvE_EEbRNS_11unique_lockINS_5mutexEEERKNS2_10time_pointIT_T0_EET1_ + 73 (__mutex_base:438)
    7   librealsense2.2.48.0.dylib     0x000000010aaf1b67 _ZNSt3__118condition_variable8wait_forIxNS_5ratioILl1ELl1000EEEZN21single_consumer_queueIN12librealsense12frame_holderEE7dequeueEPS6_jEUlvE_EEbRNS_11unique_lockINS_5mutexEEERKNS_6chrono8durationIT_T0_EET1_ + 103 (__mutex_base:482)
    8   librealsense2.2.48.0.dylib     0x000000010aaf1a2b single_consumer_queue<librealsense::frame_holder>::dequeue(librealsense::frame_holder*, unsigned int) + 107 (concurrency.h:95)
    9   librealsense2.2.48.0.dylib     0x000000010aae2d13 single_consumer_frame_queue<librealsense::frame_holder>::dequeue(librealsense::frame_holder*, unsigned int) + 35 (concurrency.h:203)
    10  librealsense2.2.48.0.dylib     0x000000010aae2ce4 librealsense::pipeline::aggregator::dequeue(librealsense::frame_holder*, unsigned int) + 52 (aggregator.cpp:107)
    11  librealsense2.2.48.0.dylib     0x000000010aa757fc librealsense::pipeline::pipeline::wait_for_frames(unsigned int) + 524 (pipeline.cpp:241)
    12  librealsense2.2.48.0.dylib     0x000000010af24b1f rs2_pipeline_wait_for_frames + 319 (rs.cpp:1778)
    13  rs-capture                     0x0000000109c59021 rs2::pipeline::wait_for_frames(unsigned int) const + 65 (rs_pipeline.hpp:513)
    14  rs-capture                     0x0000000109c5886e main + 286 (rs-capture.cpp:30)
    15  libdyld.dylib                 0x00007fff203acf5d start + 1

     

    0
    Comment actions Permalink

Please sign in to leave a comment.