David Thevenin
- Total activity 7
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by David Thevenin-
David Thevenin commented,
Hi JesusI do not have PC, only Macs. I do consider Linux into a Virtual Machine, but it looks to me a bit complicated. I'm evaluating the solution tho. But for now I'm still considering to return t...
-
David Thevenin commented,
Hi Jesus I understand; thanks for the investigation and the summary. I did test on a fresh installed macOS, means that kextstat | grep -v apple return nothing, and it does not work too. Anyway, ...
-
David Thevenin commented,
Hi Jesus Thanks. If it can help, I could test the pull request on my Mac. Bests David
-
David Thevenin commented,
Hi Jesus Garcia Do you have update on that issue?Because of this bug, I can't use the cameras on MacOS; it's blocking. In the time being I could down grade to a previous version of the SDK for inst...
-
David Thevenin commented,
Thanks here more information related to the installation: macOS 10.57.7libusb 1.0.23pkg-config 0.29.2_3glfw 3.3.2 Regards
-
David Thevenin created a post,
EXC_BAD_ACCESS On MacOS
Hi I just received my L515 camera and I'm trying to run some code examples on MacOS. For instance I'm able to compile rs-hello-realsense, but when it comes to run the example I have an exception EX...