RealSense Support

USB SCP overflow

Comments

14 comments

  • Alexandra Ciuriuc

    Hello Erdynieve, 

     

    Thank you for your interest in the Intel RealSense D435 and T265 cameras. 

    Are you using the T265 camera with the cable that came in the box? Also, are you connecting it to a USB 3 port? 

    Another user reported receiving  the "incomplete frame" error and it was due to his board overheating. Also, in the link below it is mentioned that partial frames indicate an issue with the USB sub-system. Did you try using the cameras on a different computer? 

    https://github.com/IntelRealSense/librealsense/issues/1240

     

    Regards,

    Alexandra

    0
    Comment actions Permalink
  • Erdynieve

    thanks for reply,

     

    yes, i'm using cable from the box, and i'm connecting it to USB 3 port.

    i have read your link, there they had hardware problem with overheating, i think i dont have such problem. i didnt try using the cameras on a different computer,

    and what about the first issue that i mentioned? when there's no frames received. what can you suggest?

    0
    Comment actions Permalink
  • Alexandra Ciuriuc

    Hi Erynieve,

     

    As I mentioned earlier,  partial frames indicate an issue with the USB sub-system.

    You should try using a different PC and let me know if you get the same errors.

     

    Regards,

    Alexandra

    0
    Comment actions Permalink
  • Erdynieve

    i tried using a different PC and i've got the same errors. I suppose problem with the cable. I will try buy new one and let you know whether everything work fine or not

    0
    Comment actions Permalink
  • Erdynieve

    i have got new cable, at the beginning i saw hardware notification "Incomplete video frame" two times

     

    after that, i had long period with no notification, when everything was working fine, even when i connected t265 camera

    0
    Comment actions Permalink
  • MartyG

    I'm very glad to hear you got much improved performance by changing the USB cable.   Thanks for updating us!

    Though your case of incomplete frames therefore seems related to the USB system, it is worth adding here for the reference of future readers with the incomplete frames problem that in addition to temperature also being a potential cause of such frames (as Alexandra said), Dorodnic the RealSense SDK Manager added that they can also occur when the CPU is at 100% utilization.

    Good luck with your projects! 

    0
    Comment actions Permalink
  • Wangtiandong

    I have the same problem. USB SCP overflow sometimes occurs when I do the following steps:

    1. start the pipeline by runnning pipe.start();

    2. close my program immediately without running pipe.stop().

    3. running the Realsense viewer and sometimes I will see USB SCP overflow

    Although replug USB cable can solve the problem, I want to know how can I detect this problem whithout running the RealSense Viewer?

    0
    Comment actions Permalink
  • MartyG

    Do the errors stop if you reduce the resolution or the FPS speed please?

    0
    Comment actions Permalink
  • Lemekec321

    benefits of 5G for businesses will have a great impact within the business world – no matter what sector your business is in. That’s why you must be prepared for the introduction.

    https://www.fieldengineer.com/blogs/how-businesses-can-prepare-for-5g

    -1
    Comment actions Permalink
  • MartyG

    IGNORE SPAM AD ABOVE

    0
    Comment actions Permalink
  • Charlie Harrisoon

    I faced a similar problem and this trick helped me solve it, thanks a lot.


    You can buy youtube subscribers to quickly increase their amount. 


    0
    Comment actions Permalink
  • Jakeostin34

    Thank you for sharing your post about USB SCP overflow. It is very useful for me. I have learned new information. I think you should write more detailed article about it

    I will be able to buy instagram followers to enlarge their amount

    0
    Comment actions Permalink
  • MartyX Grover

    IGNORE SPAM ADS ABOVE

    0
    Comment actions Permalink
  • Nillremilton

    wer and sometimes I have problem with d435. I see that no frames

    0
    Comment actions Permalink

Please sign in to leave a comment.