USB SCP overflow
| Camera Model | D435 |
| Firmware Version | 05.11.11.100 |
| Operating System & Version | Linux (Ubuntu 16.04) |
| Kernel Version (Linux Only) | 4.15.0-55-generic |
| Platform | PC |
| SDK Version | 2.25.0 |
| Language | --- |
| Segment | Robot |
I use two cameras d435 and t265.
I run realsense-viewer and sometimes I have problem with d435. I see that no frames received and red messages on top-right.

Also, sometimes, when it works totally fine, i see notification that "Incomplete video frame detected"

How can i get rid of "USB SCP overflow"?
-
Hello Erdynieve,
Thank you for your interest in the Intel RealSense D435 and T265 cameras.
Are you using the T265 camera with the cable that came in the box? Also, are you connecting it to a USB 3 port?
Another user reported receiving the "incomplete frame" error and it was due to his board overheating. Also, in the link below it is mentioned that partial frames indicate an issue with the USB sub-system. Did you try using the cameras on a different computer?
https://github.com/IntelRealSense/librealsense/issues/1240
Regards,
Alexandra
-
thanks for reply,
yes, i'm using cable from the box, and i'm connecting it to USB 3 port.
i have read your link, there they had hardware problem with overheating, i think i dont have such problem. i didnt try using the cameras on a different computer,
and what about the first issue that i mentioned? when there's no frames received. what can you suggest?
-
I'm very glad to hear you got much improved performance by changing the USB cable. Thanks for updating us!
Though your case of incomplete frames therefore seems related to the USB system, it is worth adding here for the reference of future readers with the incomplete frames problem that in addition to temperature also being a potential cause of such frames (as Alexandra said), Dorodnic the RealSense SDK Manager added that they can also occur when the CPU is at 100% utilization.
Good luck with your projects!
-
I have the same problem. USB SCP overflow sometimes occurs when I do the following steps:
1. start the pipeline by runnning pipe.start();
2. close my program immediately without running pipe.stop().
3. running the Realsense viewer and sometimes I will see USB SCP overflow
Although replug USB cable can solve the problem, I want to know how can I detect this problem whithout running the RealSense Viewer?
-
benefits of 5G for businesses will have a great impact within the business world – no matter what sector your business is in. That’s why you must be prepared for the introduction.
https://www.fieldengineer.com/blogs/how-businesses-can-prepare-for-5g
-
I faced a similar problem and this trick helped me solve it, thanks a lot.
You can buy youtube subscribers to quickly increase their amount. -
Thank you for sharing your post about USB SCP overflow. It is very useful for me. I have learned new information. I think you should write more detailed article about it
I will be able to buy instagram followers to enlarge their amount -
wer and sometimes I have problem with d435. I see that no frames
Please sign in to leave a comment.

Comments
14 comments