View my account

D435 example code problems

Comments

7 comments

  • Alexandra Ciuriuc

    Hi Marcjjchoo,

     

    Thank you for your interest in the Intel RealSense D435 camera. 

    Can you please run rs-enumerate-devices and provide the output?

     

    Regards,

    Alexandra

    0
    Comment actions Permalink
  • Marcjjchoo

    Hi, thanks for the help!

    Here's the output.

    Device info:
    Name : Intel RealSense USB2
    Serial Number : 915112070746
    Firmware Version : 05.11.06.250
    Recommended Firmware Version : 05.11.06.250
    Physical Port : /sys/devices/platform/soc/3f980000.usb/usb1/1-1/1-1.4/1-1.4:1.0/video4linux/video0
    Debug Op Code : 15
    Advanced Mode : YES
    Product Id : 0AD6
    Usb Type Descriptor : 2.1
    Product Line : D400
    Asic Serial Number : 901313020365

    Stream Profiles supported by Stereo Module
    Supported modes:
    stream resolution fps format
    Infrared 1 1280x720 @ 6Hz Y8
    Infrared 1 640x480 @ 30Hz Y8
    Infrared 1 640x480 @ 15Hz Y8
    Infrared 1 640x480 @ 6Hz Y8
    Infrared 1 480x270 @ 60Hz Y8
    Infrared 1 480x270 @ 30Hz Y8
    Infrared 1 480x270 @ 15Hz Y8
    Infrared 1 480x270 @ 6Hz Y8
    Depth 1280x720 @ 6Hz Z16
    Depth 640x480 @ 30Hz Z16
    Depth 640x480 @ 15Hz Z16
    Depth 640x480 @ 6Hz Z16
    Depth 480x270 @ 60Hz Z16
    Depth 480x270 @ 30Hz Z16
    Depth 480x270 @ 15Hz Z16
    Depth 480x270 @ 6Hz Z16

    0
    Comment actions Permalink
  • Marcjjchoo

    I've also added a screenshot of the realsense viewer in operation

    0
    Comment actions Permalink
  • Alexandra Ciuriuc

    Hi Marcjjchoo,

     

    Can you please send screenshots of the exact errors you are receiving?

    Also, please keep in mind that support for Raspberry Pi and USB2 is experimental which means that many features will not work and there is severely reduced functionality.

     

    Regards,

    Alexandra

    0
    Comment actions Permalink
  • Marcjjchoo

    Hi, on the top left terminal I'm trying out the compiled cpp executables, on the bottom left terminal I'm running the python examples, on the bottom right I ran python code line by line to show that the runtime error occurs at pipeline.start().

    0
    Comment actions Permalink
  • Marcjjchoo

    Btw, as additional information, I built librealsense with "cmake ../ -DBUILD_EXAMPLES=true"

    I also built pyrealsense from source since pip install pyrealsense2 resulted in:

    Looking in indexes: https://pypi.org/simple, https://www.piwheels.org/simple
    Collecting pyrealsense2
    ERROR: Could not find a version that satisfies the requirement pyrealsense2 (from versions: none)
    ERROR: No matching distribution found for pyrealsense2

    0
    Comment actions Permalink
  • Alexandra Ciuriuc

    Hi Marcjjchoo,

     

    Can you please tell me if you followed these instructions exactly?

    https://github.com/IntelRealSense/librealsense/blob/master/doc/installation_raspbian.md

     

    Regards,

    Alexandra

    0
    Comment actions Permalink

Please sign in to leave a comment.