Marcjjchoo

  • Total activity 6
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Marcjjchoo
  • Marcjjchoo commented,

    Btw, as additional information, I built librealsense with "cmake ../ -DBUILD_EXAMPLES=true" I also built pyrealsense from source since pip install pyrealsense2 resulted in: Looking in indexes: http...

  • Marcjjchoo commented,

    Hi, on the top left terminal I'm trying out the compiled cpp executables, on the bottom left terminal I'm running the python examples, on the bottom right I ran python code line by line to show tha...

  • Marcjjchoo commented,

    I've also added a screenshot of the realsense viewer in operation

  • Marcjjchoo commented,

    Hi, thanks for the help! Here's the output. Device info: Name : Intel RealSense USB2Serial Number : 915112070746Firmware Version : 05.11.06.250Recommended Firmware Version : 05.11.06.250Physical Po...

  • Marcjjchoo created a post,

    D435 example code problems

    Camera Model: D435 Firmware Version: 5.11.6 Operating System Version: Ubuntu Mate 18.04 Kernel Version (Linux Only): 4.15 Platform: Raspberry Pi 3B SDK Version: 2.24.0 Language: python3/ C++ I...