Error (9901) : from Dynamic Calibration Tool and CustomRW.
Hello,
I have more than 20 D435 cameras. However, most cameras don't have extrinsic parameters between color and depth, which makes color-depth alignment impossible.
So, I've been trying to re-calibrate many D435 cameras using Dynamic Calibrator and CustomRW. However, these two tools provide me the same response as below:
"Error (9901): calibration tables on device are not supported, Please try again with latest Dynamic Calibrator software.
If you are already using latest software, please re-calibrate the device with latest OEM Calibration tools and try again.
check CustomRW tool."
How Can I fix this problem? Is purchasing Intel® RealSense™ D400 Camera OEM Calibration Target the only way to solve it?
If I purchase an OEM Calibration Target, Can I get the OEM calibration tool?
Is there any limit to the OEM calibration tool, such as the limited number of cameras that can be calibrated?
I appreciate any help you can provide.
Please sign in to leave a comment.
Comments
1 comment