RealSense Support

Move d435 RGB sensor and align to depth

Comments

15 comments

  • MartyG

    Hi Maxime Ambard Thanks very much for your questions.

     

    1. Yes, the HSF interposer cables - available in the official RealSense Store - will connect the Vision Processor D4 Board to your D430 board.  The number in the cable name refers to its length in mm (50 mm and 100 mm) - they are both equal quality.

     

    2.  A company called Cocom Consumer Logistics may be worth contacting regarding ordering a custom cable for the RGB sensor, as they are the recommended logistics source for custom interposer cable queries in the official data sheet document for the RealSense 400 Series cameras.

     

     

    3.  The official RealSense Dynamic Calibration software tool can be used to calibrate both the depth and RGB sensors.  You can download the tool for Windows from the link below or use instructions on page 14 onwards of the tool's user guide document to install it on Ubuntu.

    https://www.intel.com/content/www/us/en/download/645988/intel-realsense-d400-series-dynamic-calibration-tool.html

     

    0
    Comment actions Permalink
  • Yaser Jay

    Hello,
    I am using the D430 camera with the D4 mainboard connected to an RGB camera via HSF50, and I calibrated it using the software provided in the link you gave me. However, the calibration failed and encountered an issue.
    The error code is 9901,
    "#16:initialize dynamic calibration parameters .
    #17: Start Initialize device ..
    #18: initialization failed.
    #19: Error (9901): calibration tables on device are not supported, please try again with latest Dynamic calibrator software.
    If you are already using latest software, please re-calibrate the device with latest OEM calibration tools and try again.
    check CustomRw tool.
    #20: Failed to start calibration"
    How can I solve this problem?

    0
    Comment actions Permalink
  • MartyG

    Hi Yaser Jay  This error has been encountered previously by a couple of other RealSense users.  Guidance about the error written by Intel offers the advice below to attempt to correct the problem using the CustomRW software that is provided with the Dynamic Calibration software.

     

    1.  Launch the CustomRw tool with the command Intel.Realsense.CustomRW -r to output the calibration tables.

    2.  Then input Intel.Realsense.CustomRW -g to recover the calibration table.

    3.  And finally, attempt the Dynamic Calibration again to confirm that the recovery worked.

     

    Unless you are going to be performing depth-color alignment then it is possible that you will not need to calibrate the RGB sensor.  And you can calibrate depth using the alternative On-Chip Calibration tool.

    https://dev.intelrealsense.com/docs/self-calibration-for-depth-cameras

     

    If you are able to use Python programming code then an alternative approach to performing a Dynamic Calibration would be to define custom calibration values that are stored in the computer's memory instead of being written to the camera hardware by the calibration tool. Here is an example of Python scripting for doing so:

    https://github.com/IntelRealSense/librealsense/issues/4061

    0
    Comment actions Permalink
  • Yaser Jay

    Yes, I am currently performing depth and color alignment.
    My camera was originally a d430, but it was identified as a d435 due to the addition of a separate RGB. I suspect there is an issue with the internal information.
    At the same time, I have used CustomRW for error correction as you suggested, but there is still a problem, and the error code is still 9901.
    (I am currently using Windows 11. If you need Ubuntu, please let me know. Thank you)

    0
    Comment actions Permalink
  • MartyG

    There is not an existing documented case to refer to where there was a successful outcome reported when dealing with this Dynamic Calibration tool error.

     

    There are two main ways of performing depth-color alignment - align_to (like in the SDK example program 'rs-align') or mapping depth and RGB together into a pointcloud (the 'rs-pointcloud' example).

     

    As you have the Windows version of the RealSense SDK installed, have you checked whether depth and RGB are able to correctly align together in either the rs-align or rs-pointcloud programs without having first calibrated the separate RGB sensor, please?

     

    You can find the location of the example programs of the Windows SDK by right-clicking on the RealSense Viewer launch shortcut icon on the Windows desktop and selecting 'Open file location' from the drop-down menu.

    0
    Comment actions Permalink
  • Yaser Jay

    Thank you for your suggestion.
    I tried rs-align.exe again, and it can display both depth and color maps. However, there is a problem with the output of rs-pointcloud.exe. From the results, it seems that the depth and color maps are not correctly unified.

    0
    Comment actions Permalink
  • MartyG

    The RealSense Viewer's 3D pointcloud mode uses the same depth-RGB mapping method as rs-pointcloud.  Could you open the Viewer please and click on the 3D option in the top-right corner of the Viewer window to make sure that you are in pointcloud mode, and then enable the depth stream (Stereo Module) first and the RGB second.  Depth and RGB should then automatically align together.

     

    If they map together in the Viewer okay, this will indicate that the alignment problem is with the rs-pointcloud program specifically rather than the map_to alignment method in general.

    0
    Comment actions Permalink
  • Yaser Jay

    OK, I have carried out the relevant operations as required, but judging from the results, the depth and color are still not aligned, and the colors in the 3D image are chaotic.

    0
    Comment actions Permalink
  • Yaser Jay

    3D option in the top-right

    0
    Comment actions Permalink
  • MartyG

    Thank you very much for your tests.  Does your project require a 3D pointcoud image or would a non-pointcloud aligned depth-RGB image like that from rs-align be sufficient?

     

    If you do require a pointcloud, please next try aligning depth to the infrared image in the Viewer instead of RGB, since the Infrared image is effectively like a monochrome RGB image.  You can do this by enabling the Infrared stream in the Stereo Module settings before you enable the Stereo Module, and then go to the Texture option at the top of the Viewer in pointcloud mode and select Infrared as the texture instead of RGB color.  

     

    Do depth and Infrared images perfectly align?  They should as they both originate from the same depth sensor.

    0
    Comment actions Permalink
  • Yaser Jay

    My project involves drone tracking, requiring the use of the d435 camera in conjunction with the YOLO algorithm to achieve object tracking. Therefore, I need to align the color image and depth map, so that I can use YOLO to determine the distance information of the recognized objects. At the same time, I also need to run VINS-fusion with this camera, so RGB texture alignment is crucial.
    :(

    0
    Comment actions Permalink
  • MartyX Grover

    If depth and the separate RGB align correctly with the non-pointcloud 'rs-align' then they are likely going to align okay with YOLO and VINS-Fusion too based on my (admittedly limited) knowledge of using RealSense cameras with those applications.  Would it be possible for you to perform tests with YOLO or VINS-Fusion and let me know the outcome of the tests later?

    0
    Comment actions Permalink
  • Yaser Jay

    OK, I'll test again

    0
    Comment actions Permalink
  • Yaser Jay

    I found that the problem I encountered is basically the same as the one in this link. D435 with new d4 will fuse depth and rgb in black pointcloud and dynamic calibr. tool doesn't work · Issue #7300 · IntelRealSense/librealsense
    The color image and the point cloud cannot be aligned. May I ask if there is a solution now?
    In any case, thank you again.

    0
    Comment actions Permalink
  • MartyG

    In that particular case, the user experienced the error when replacing the Vision Processor D4 board inside a D435 camera with a new D4 board.  So their camera would have been using the original RGB sensor and be in its normal position, meaning that it should not have needed a calibration to take account of a new RGB sensor position.

     

    The calibration table is stored on the D4 board and not the D430 depth module.

     

    I would recommend creating a new issue about this problem on the RealSense GitHub support website.  The issue can then be highlighted to members of the RealSense team to identify a way forward.  You can do this by clicking on the green 'New Issue' button on this page:

    https://github.com/IntelRealSense/librealsense

    0
    Comment actions Permalink

Please sign in to leave a comment.