Depth Camera baseline
I can see that in every intel depth camera the baseline of the 2 sensor has been given. It is always a default distance for the baseline in all depth sensors or it can be adjusted in some cases or cameras?
-
Hi Dimouzoi On the RealSense 400 Series cameras the baseline is the horizontal distance between the center-line of the left and right infrared sensors on the front of the camera. The length of the baseline is fixed and cannot be changed.
-
As the baseline between different camera models vary, you can select a particular model for a particular benefit. For example, the very short baseline on the D405 model provides high accuracy, high quality images at very close range. The D415 has higher quality / better accuracy images than the D435 models, though it has a smaller field of view and so can see less of a scene's contents. D455's wide baseline can provide longer range depth sensing than the D435 models.
Intel cannot provide advice about non-RealSense depth cameras.
Please sign in to leave a comment.
Comments
3 comments