RealSense Support

Intel renascence working issue

Comments

5 comments

  • MartyG

    Hi Chandiran  When you mention 'dual sensor', do you mean two separate cameras (the D410 and another camera).  If so then Raspberry Pi single-board computers usually have only one RealSense camera attached per Pi board. 

     

     

    Other single-board computer types such as Nvidia Jetson and Up Squared are better suited to having more than one camera attached and operating simultaneously.

    0
    Comment actions Permalink
  • Chandiran
    Dear MartyG,
     
    Thanks for the information.
     
    We are using RPI 4 Model B series of SBC which has 4G/8GB RAM, 04 USB Port (2.0 & 3.0), Gigabit Ethernet, also has package of H.265 decoder, 1080p30 encoder, Open GL ES 3.1 , Vulkan 1.0.
    Linux kernel : 5.10.63-v7l+
    Intel SDK compatible version:
     
    Moreover our end application requires only to capture IR & depth frames with 30FPS from 02 sensors.
     
    Kindly suggest what are the recommended specs for COTS/Custom SBC to work with 02 Intelsensor simultaneously connected to single SBC.
     
    Regards
    chandiran.S
    0
    Comment actions Permalink
  • MartyG

    Aside from the mentioned Nvidia Jetson and Up SBC boards that are known to work with two RealSense cameras (and also Intel NUC computing products), it is difficult to provide recommendations for specific board products that can support multiple cameras. 

     

    A general rule of thumb that I use for specifications is capability equal to Intel Core i3 computers for 2 simultaneously active cameras, Core i5 for 3 cameras and Core i7 / i9 for 4 or more cameras.

    0
    Comment actions Permalink
  • Chandiran
    Dear MartyG,
     
    Thanks for the information.
     

    The Raspberry Pi 4 B (Broadcom BCM2711) processor has similar performance benchmarks to the Intel Core i3, as shown in the comparison links provided.(https://www.cpu-monkey.com/en/compare_cpu-raspberry_pi_4_b_broadcom_bcm2711-vs-intel_core_i3_4130 ) and (https://cpu-compare.com/cpu/compare/raspberry_pi_4_b_broadcom_bcm2711-vs-intel_core_i3-4160t).

    Therefore, like the Intel Core i3, the Raspberry Pi 4 B should be capable of connecting 2 active cameras. Moreover, when running 2 cameras, the Raspberry Pi 4 B has an average CPU load of 30-40%, indicating it has sufficient resources to handle dual camera streaming.

    Regards

    Chandiran.S

    0
    Comment actions Permalink
  • MartyG

    Thank you for the data.

     

    Are you using the official 1 meter long USB cable supplied with the camera or a longer USB cable of your own choice, please?

    0
    Comment actions Permalink

Please sign in to leave a comment.