Chandiran
- Total activity 4
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Chandiran-
Chandiran commented,
Dear MartyG, Thanks for the information. The Raspberry Pi 4 B (Broadcom BCM2711) processor has similar performance benchmarks to the Intel Core i3, as shown in the comparison links provided.(ht...
-
Chandiran commented,
Dear MartyG, Thanks for the information. We are using RPI 4 Model B series of SBC which has 4G/8GB RAM, 04 USB Port (2.0 & 3.0), Gigabit Ethernet, also has package of H.265 decoder, 1080p30 enc...
-
Chandiran created a post,
Intel renascence working issue
hi, I am currently utilizing the Intel-renascence D410 on Raspberry Pi 4B, which has 4GB of RAM and runs on Raspbian GNU/Linux 10 (buster). Additionally, I am using SDK 2.50.0 and the intel-renasce...