D435 USB suddenly unrecognizable
I have been using Realsense D435 with Ubuntu20.04 on Intel NUC11. It has been working for 3month and suddenly, it became unrecognizable on Hardware basis. No device files created. Also Other Windows PCs cannot recognize even as an USB device. Never can be restored.
I have benn suffring this and it happened 4 times. four broken D435s lol.
Have anyone suffering the same thigs? or have any thoughts?
-
Hi Asano,
Thanks for reaching out to us.
Could you please try the following suggestions and see if your Windows PCs can recognize the cameras?
-
Use the latest firmware and RealSense SDK 2.0 version.
-
Connect the camera directly to a USB 3 port on your PC.
If the camera is already connected directly to the PC, try using a powered USB hub.
-
Use the USB cable that came with the RealSense camera.
The cable that came with your RealSense Camera is a high-quality USB cable that is capable of handling the power and bandwidth requirements of the camera. Using other cables is not recommended.
-
Flip the USB C connector that is inserted into the camera and re-insert it the opposite way.
Sometimes the camera will work only if the cable is inserted in a particular orientation.
-
Update the USB drivers on the PC.
You probably already have the latest USB drivers due to automatic Windows Updates but this is worth checking.
Regards,
Wan
-
Use the latest firmware and RealSense SDK 2.0 version.
Please sign in to leave a comment.




Comments
8 comments