View my account

D435 USB suddenly unrecognizable

Comments

8 comments

  • Wai Fook Wan

    Hi Asano,

    Thanks for reaching out to us.

    Could you please try the following suggestions and see if your Windows PCs can recognize the cameras?

    1. Use the latest firmware and RealSense SDK 2.0 version.
       
    2. Connect the camera directly to a USB 3 port on your PC.
      If the camera is already connected directly to the PC, try using a powered USB hub.
       
    3. Use the USB cable that came with the RealSense camera.
      The cable that came with your RealSense Camera is a high-quality USB cable that is capable of handling the power and bandwidth requirements of the camera. Using other cables is not recommended.
       
    4. Flip the USB C connector that is inserted into the camera and re-insert it the opposite way.
      Sometimes the camera will work only if the cable is inserted in a particular orientation.
       
    5. Update the USB drivers on the PC.
      You probably already have the latest USB drivers due to automatic Windows Updates but this is worth checking.

     

    Regards,

    Wan

    0
    Comment actions Permalink
  • Asano

    dear Wan

    thank you. but our realsense are not even recognizable by windows even if we update Windows' driver.

    we are using USB3.0 hub. do you have any recommendation which one we can use?

    0
    Comment actions Permalink
  • Wai Fook Wan

    Hello Asano​, 

    We'll handle this issue via a private ticket. 

     

     

    Regards, 

    Wan

    0
    Comment actions Permalink
  • Asano

    0
    Comment actions Permalink
  • Asano

    realsense is connected but not recognized

     

    0
    Comment actions Permalink
  • Asano

    0
    Comment actions Permalink
  • Asano

    these are new OK realsense connected

     

    0
    Comment actions Permalink
  • Wai Fook Wan

    Hello Asano,
    Thanks for the information.
    Based on your screenshot, the camera is faulty and needs to be returned.
    I've contacted you via Zendesk with ticket number #21473, and we'll continue our conversation there.


    Regards,
    Wan

    0
    Comment actions Permalink

Please sign in to leave a comment.