RealSense Support

Position of Camera for Moving Object Reconstruction

Comments

2 comments

  • MartyG

    Hi Javier Recasens  As the camera is pointing straight down, the orientation should not make a difference to performance.  The main influence that the orientation is likely to have is how much of the vehicle is captured in the camera's field of view, which is 87° × 58°. 

     

    As the horizontal size of the field of view is wider than the vertical field of view, having the camera oriented on its side would likely be optimal.  This is because the car will be lengthy along the horizontal FOV and shorter along the vertical FOV, so a side-on camera orientation should have a much better chance of capturing the entire car within the FOV.

     

    0
    Comment actions Permalink
  • Javier Recasens

    As always, Thanks Marty.

    A side-on camera orientation (or camera being parallel to the object's movement direction) makes sense, I can use less frames for the reconstruction.

    0
    Comment actions Permalink

Please sign in to leave a comment.