Javier Recasens

  • Total activity 14
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 4

Activity overview

Latest activity by Javier Recasens
  • Javier Recasens commented,

    I was able to make it work. Device must be enabled and streaming. Example: https://github.com/IntelRealSense/librealsense/issues/866

  • Javier Recasens commented,

    What I find most strange is that the sensor does support some of the temperature options (such as <option.asic_temperature: 23> and <option.projector_temperature: 25>: sensor.get_supported_options(...

  • Javier Recasens created a post,

    No Temperature enabled for D457 (Python)

    Im using a D457 camera but it looks like there is no support for any of the temperature readings when using pyrealsense2. HW Firmware: 5.15.0.2pyrealsense2 (2.54.1.5217) ...sensor = profile.get_dev...

  • Javier Recasens commented,

    You could use an interval of quantiles (e.g. 5% to 95%) to set all pixel depth values outside that range to zero (or impute with the median or nearest neighbor).  

  • Javier Recasens commented,

    As always, Thanks Marty. A side-on camera orientation (or camera being parallel to the object's movement direction) makes sense, I can use less frames for the reconstruction.

  • Javier Recasens created a post,

    Position of Camera for Moving Object Reconstruction

    Hello, I’m using a fixed D457 camera to capture the top section of a moving object for 3D reconstruction. I'm curious about the optimal camera positioning to improve triangulation in stereo matchin...

  • Javier Recasens commented,

    MartyG Could we get confirmation that the USB Type-C connector (Female Receptacle) of the D457 camera is waterproof? To ensure waterproof capabilities in the D457 camera, it is important to conside...

  • Javier Recasens commented,

    Thanks. I think the IP68 product I could use are: Amphenol LTW UC30ML-NCML-QB001 Bulgin PXP4040/C/A/1M00 I wonder if these are recommended cables... My concern is that they do not have "Screw Locki...

  • Javier Recasens created a post,

    D457 - Waterproof USB-C connection

    Hello, I need assistance in protecting the USB-C connection of the D457 camera that I plan to use outdoors. The camera has an IP65 rating, which should protect it from dust and projected water. How...