D457 - Waterproof USB-C connection
Hello, I need assistance in protecting the USB-C connection of the D457 camera that I plan to use outdoors. The camera has an IP65 rating, which should protect it from dust and projected water. However, I've noticed a gap in the connection that may compromise its waterproofing. Are there any recommended covers or sealants commonly used for IoT installations to enhance water protection? Thanks in advance.
-
Hi Javier Recasens You can use your own choice of USB Type-C cable with RealSense cameras so long as it is a high-quality cable. There are USB cables available with IP68 rated connectors that are waterproof and dustproof. For more information, please google for the term usb-c ip68
-
Thanks. I think the IP68 product I could use are:
Amphenol LTW UC30ML-NCML-QB001
I wonder if these are recommended cables... My concern is that they do not have "Screw Locking" which is available in the D457:

-
The most important factor is the cable quality, not using an inexpensive charging / sync one but a high quality one suited to data transfer. This is because of the high volume of data that RealSense cameras can transmit. Amphenol are a leading electronics brand.
For RealSense-validated USB products, Newnex can also be recommended.
-
MartyG Could we get confirmation that the USB Type-C connector (Female Receptacle) of the D457 camera is waterproof?
To ensure waterproof capabilities in the D457 camera, it is important to consider both the USB Type-C connector and the enclosure. Simply having a waterproof enclosure does not guarantee that the USB-C camera connector itself is waterproof.
I am afraid that buying a waterproof USB-C cable may not be enough. For complete assurance of waterproof functionality, it is necessary to ensure that both the USB-C connector and the corresponding plug have the appropriate IP (Ingress Protection) rating.
BTW, I contacted Newnex and they do not have any water proof USB cables for the D457.
-
Marty, The visual inspection of tightness alone cannot ensure the IP65 rating. Although I purchased waterproof cables from reputable brands like Amphenol and Bulgin, it's crucial to note that all these cables necessitate a waterproof receptacle for proper functionality (they are only waterproof when mated). This underscores the significance of waterproofing the female USB-C connection of the D457.
It's worth considering whether the creators of the D457 enclosure designed the accompanying plate to facilitate the attachment of a waterproof receptacle

Since such a waterproof plate in the USB-C location does not exist, I believe the only solution would be to create a custom waterproof part to replace it (and customize the mating for other brands such as Amphenol and Bulgin).


However, customization will be a challenge since the CAD model does not have the USB plate as shown above. Only the outside surface is available (not a volume or mesh with the internal extrusion). Details on the USB rubber gasket are also not available online nor in the datasheet.
I am surprised the D457 is being marketed as IP65 if we cannot really protect the USB connection from "water jets from any direction".
-
If you would prefer to add an extra layer of waterproof USB protection without having to find or make a seal that fits perfectly and the USB connector will not need to be removed from the port of the camera, inserting it and then wrapping waterproof tape around the connector might be sufficient.
-
Thanks for the recommendation MartyG.
Would you recommend using Clear Silicone Waterproof Sealant? (e.g. Loctite 908570)
-
A sealant around the outside of the USB port instead of waterproof tape could be a solution.
I cannot offer a recommendation for a specific product but if you check that a sealant is IP68 rated (waterproofed against submersion instead of just water spray) then it should be fine. You could do this by googling the product's name and adding "ip68" to the search term in quotation marks to ensure that this exact term must be in the search result to ensure relevancy.
Please sign in to leave a comment.
Comments
9 comments