RealSense Support

Sync RGB and Depth Data on L515

Comments

3 comments

  • Zulkifli Halim

    Hello Katharina,

     

    Thank you for contacting us.

     

    The synchronization between two streams from the same sensor like depth and IR should be perfectly synchronized by frame number.

     

    Synchronization between two streams from separated sensors, like color and depth, is achieved by the best match of the timestamp of the frame, It’s expected that frames within a synchronized frameset will have a temporal offset, bounded by a period of one frame with the lowest FPS.

     

    Regards,
    Zulkifli Halim
    Intel Customer Support

    0
    Comment actions Permalink
  • Katharina

    Do you synchronize the frames based on the best match of the timestamp (as you described) when I request "aligned" data? That is either color aligned with depth or depth aligned with color? Can I assume that the aligned frames are already optimized for the best match of timestamps when I receive them using your SDK?

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Katharina,

     

    The above assumes that there are no frame drops. 

     

    Regards,

    Zulkifli

    0
    Comment actions Permalink

Please sign in to leave a comment.