Katharina
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by Katharina-
Katharina commented,
Hi Zulkifli, When I launch the RealSense Viewer, the preset does not automatically set to default. It automatically sets to "Max Range" and when I look at all the options in the drop-down menu, "De...
-
Katharina commented,
Do you synchronize the frames based on the best match of the timestamp (as you described) when I request "aligned" data? That is either color aligned with depth or depth aligned with color? Can I a...
-
Katharina commented,
I can't see "Default" as an option anymore when I launch the Intel Realsense Viewer. The only options I have are: Custom No Ambient Light Low Ambient Light Max Range Short Range Is "Default" simi...
-
Katharina created a post,
Sync RGB and Depth Data on L515
Hi, I want to use the L515 on a mobile robot, but am noticing that the RGB data is lagging behind the depth data, despite them both being "published" at 30 fps. Is there a way to sync them such th...
-
Katharina commented,
Thanks for the answer! The link to the rs_options.h file is really helpful. I also managed to build the intel realsense viewer for OSx and was able to test some of the configurations. Are those con...
-
Katharina created a post,
Configure L515 camera without Windows computer
I am working with the L515, but the quality of the depth data is poor for our purposes. After doing some research, it seems like I can improve the data by configuring the camera. From what I unders...