View my account

Measure option in Realsense Viewer

Comments

3 comments

  • MartyX Grover

    Hi Varsha 11891  A reason why the Measure option in the 3D mode of the RealSense Viewer may be disabled is if the GLSL options in the 'Performance' section of the Viewer's Settings page are disabled.  

     

     

    You can access the Settings interface by left-clicking on the gear-wheel icon in the top corner of the Viewer window and selecting Settings from its drop-down menu.  Then left-click on the Performance tab of the Settings overlay that pops up to locate the GLSL options.

    0
    Comment actions Permalink
  • Varsha 11891

    Thank you so much for the quick response @MartyG. I'm afraid im not able to see that option under the performance tab. Is there another alternative?

    0
    Comment actions Permalink
  • MartyX Grover

    The Measure tool is available as a standalone SDK example program outside of the Viewer.  

    https://github.com/IntelRealSense/librealsense/tree/master/examples/measure

    I am not aware of an alternative means to access the Measure tool from within the Viewer if the GLSL options are not available though.

    0
    Comment actions Permalink

Please sign in to leave a comment.