RealSense Support

About the camera connection issue on ROS

Comments

5 comments

  • MartyX Grover

    Hi Getomboy  The initial_reset instruction is a launch command that resets the camera at launch and can be activated from the roslaunch instruction or defined in the launch file.  

    If the camera is able to be detected successfully during a launch but it is not launching succesfully every time then there is certainly no harm in including an initial_reset instruction in the launch configuration to see whether it increases your launch reliability further.

    0
    Comment actions Permalink
  • Getomboy

    Excuse me. Could you have the specific approach?

    Such as SOP of the resetting parameter.

    I cannot catch your solution.

    Or the machine is broken ?

    Thanks again.

    0
    Comment actions Permalink
  • MartyX Grover

    Your RealSense ROS wrapper installation is likely okay if it is able to launch successfully.  It is just a matter of increasing the reliability of launch.  Please try launching with the roslaunch instruction and adding this command to the end of your roslaunch instruction:

    initial_reset:=true

     

    For example:

    roslaunch realsense2_camera rs_camera.launch initial_reset:=true

    0
    Comment actions Permalink
  • Getomboy

    Hi MartyG,

    I've used your solution that the camera has done resetting device.

    Unfortunately,  the error still exist.

    Could you have another suggestion?

    Or I need to check something?

    Thanks.

    0
    Comment actions Permalink
  • MartyX Grover

    The librealsense SDK and ROS wrapper versions that you are using are very old (from mid 2019).   Would it be possible to update your SDK and wrapper to modern versions (SDK 2.43.0 and wrapper 2.2.23) as they still support Ubuntu 16.04.

    librealsense 2.43.0

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.43.0

    ROS wrapper 2.2.23

    https://github.com/IntelRealSense/realsense-ros/releases/tag/2.2.23

     

    If it is not possible to change your versions then I would suggest looking at the camera firmware instead.  The firmware 5.12.11.0 that the log says is installed in your camera is recommended for the modern librealsense version 2.41.0

    The firmware version that is recommended for SDK 2.24.0 is 5.11.6.250 and is available from the firmware releases page.

    https://dev.intelrealsense.com/docs/firmware-releases

     

     

    Overall though, my recommendation would be to update your project computer to a modern RealSense setup if it is possible for your project:

    SDK 2.43.0

    ROS wrapper 2.2.23

    Firmware driver 5.12.12.100

    0
    Comment actions Permalink

Please sign in to leave a comment.