object dimensional measurement using depth camera(D435i)
I need dimensional measurement of object, can it be found using single depth camera or not.
-
Hi Revathi Do you need to measure between two points on the object or measure the height, width and length of the object (volumetric measurement) please?
-
Volumetric measurement is a way of describing measuring the XYZ dimensions of an object such as a box.
If you are able to use Windows or Android and do not mind commercial software then the software DotProduct Dot3D Scan can provide 3D point-to-point measurement and area / diameter / cube measurement. It is compatible with D435i.
-
If you are able to use Python, a good starting point will be to try it with the example box_dimensioner_multicam that can also work with a single camera.
Please sign in to leave a comment.


Comments
7 comments