RealSense Support

D435 not detected on windows 10

Comments

8 comments

  • MartyX Grover

    Hi O Patrouix  Do you hear the USB insertion sound effect of Windows (doo-doo-doo-doo) when inserting the camera with the problem into a USB port on your hub, please?

    If not, is there any reaction if you insert the camera into a USB port directly on the laptop?

    0
    Comment actions Permalink
  • O Patrouix

    No insertion noise through the hub or directly on the laptop.

    0
    Comment actions Permalink
  • MartyX Grover

    And there is no difference if you unplug the micro end of the cable from the side of the camera, turn it upside down and re-insert it into the camera (as USB-C cables are two-way insertion on their micro end)?

    0
    Comment actions Permalink
  • O Patrouix

    No difference. I've made 2 tests :

     - turning the USB-C cable at the camera

     - turning the USB-C cable at laptop

    The 4 possibilities have given the same result.

     

    0
    Comment actions Permalink
  • O Patrouix

    I've noticed that the camera body of the non running one is getting hotter than the running one.

    Maybe the internal voltage regulator has a problem ?

    The non running one was plugged on the USB hub with an Arduino board also plugged. The Arduino voltage regulator (external power) broke maybe because the USB was connected to the laptop and the external power was also used.

    Any feedback is welcome.

    0
    Comment actions Permalink
  • MartyX Grover

    A USB device may heat up rapidly if there is a fault in the USB cable or in the USB port.  

    There was also once a case of a developer board overheating, with accompanying camera ASIC and Projector temperatures of 60 and 56 degrees C respectively.

    https://github.com/IntelRealSense/librealsense/issues/1240#issuecomment-369065209

    0
    Comment actions Permalink
  • O Patrouix

    I'll have a look but my second D435 does not heat up on the same laptop, USB hub and cable.

    I suspect that the non running one has a problem inside.

    0
    Comment actions Permalink
  • MartyX Grover

    Please do update about your case here after having a look.  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.