O Patrouix

  • Total activity 6
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by O Patrouix
  • O Patrouix commented,

    I'll have a look but my second D435 does not heat up on the same laptop, USB hub and cable. I suspect that the non running one has a problem inside.

  • O Patrouix commented,

    I've noticed that the camera body of the non running one is getting hotter than the running one. Maybe the internal voltage regulator has a problem ? The non running one was plugged on the USB hub ...

  • O Patrouix commented,

    No difference. I've made 2 tests :  - turning the USB-C cable at the camera  - turning the USB-C cable at laptop The 4 possibilities have given the same result.  

  • O Patrouix commented,

    No insertion noise through the hub or directly on the laptop.

  • O Patrouix created a post,

    D435 not detected on windows 10

    I've got 2 D345 and one is not detected (was working but stops). On the same laptop using the same USB hub (usb-c connector) and the same cable, one is working as it should the other is not detecte...