RealSense Support

Intel Realsense D435 Depth sensing reliability and accuracy

Comments

15 comments

  • MartyX Grover

    Hi Yiherng  Would it be possible to provide an RGB and depth image of a typical scene that the camera is observing please?  This will help a lot to diagnose accuracy problems that might be being caused by environmental conditions such as lighting, or other elements in the scene that could have negative consequences for the depth image.

    0
    Comment actions Permalink
  • Yiherng

    Thanks for reply MartyG

    Please see the attached color and depth images captured by the camera. 

    0
    Comment actions Permalink
  • Yiherng

    In the above case, the depth of the bounding box is 0.46 m. Here is how I obtain the depth data,

    depth = np.asanyarray(depth_image.get_data())
    depth = depth[target_box[0]:target_box[2], target_box[1]:target_box[3]].astype(float)
    depth_scale = depth_sensor.as_depth_sensor().get_depth_scale()
    depth = depth * depth_scale
    dist = _get_depth_median(depth)
     
    I have _get_depth_median() function to get the median of the depth data. The reason of using median instead of the mean is to rule out those outliers. 
     
    So the issue here is, 40 % of the time the depth calculation is just wrong (0.6 m or 1 m or even 0m), and I need to unplug and replug the camera to get it to work normally again.  
    0
    Comment actions Permalink
  • MartyG

    Thanks very much for the useful images.

    I would expect the foreground near to the camera to be primarily colored blue.  It looks as though the surfaces that may be having their distance mis-read as orange and yellow-green (further away than they actually are) are ones that light can reflect off, such as metal and plastic bottles.  Reflections make surfaces more difficult for the camera to read depth detail from.

    In this situation, aligning depth to color may help, as it makes it easier to distinguish foreground pixels from background pixels.  Intel have examples for such alignment with Python.

    align-depth2color.py

    https://github.com/IntelRealSense/librealsense/blob/master/wrappers/python/examples/align-depth2color.py

    depth_under_water

    This Jupyter Notebook example is especially relevant, as it uses alignment to deal with reflections.

    https://github.com/IntelRealSense/librealsense/blob/jupyter/notebooks/depth_under_water.ipynb

    In regard to depth_scale, unless you are changing the value during runtime then you do not need to retrieve the value with a programming instruction in real-time as it is normally unchanging.  You can set it to a fixed numeric value of 0.001 (the default depth unit scale of the 400 Series cameras), or try 0.0001 for a potentially improved quality depth image with less missing data when performing close-range sensing like this particular application.

    You could also try putting a card background along the bottom of the rack with the triangular sections where the fiducial tag card is, as the camera may interpret the triangles as a repetitive pattern and become confused.

    A repetitive pattern is where there are elements in the scene that repeat horizontally or vertically, such as horizontal fence post rows or tree-top rows, or vertical window blinds 

    0
    Comment actions Permalink
  • Yiherng

    Now that you mentioned it, it seems really weird to me as well. I use the following method to colorize the depth frame:

    colorizer = rs.colorizer()
    depth_image = frame
    depth_image = depth_image.as_depth_frame()
    colorized_depth = np.asanyarray(colorizer.colorize(depth_image).get_data())
     
    But when I visualize it on realsense-viewer app, the colors are actually flip.

    I did use the same method as align-depth2color, as I realized FOV of stereo-vision is actually wider than RGB camera. Aligned-depth2 color is necessary otherwise the reading will always be far off. 

    0
    Comment actions Permalink
  • Yiherng

    This is what I see from realsense-viewer app.

    0
    Comment actions Permalink
  • Yiherng

    By the way, the depth scale being 0.0001 does not work as it would just make the correct depth readings even smaller. 

    0
    Comment actions Permalink
  • MartyG

    The image from the RealSense Viewer looks more correct, with the bottles, fiducial tag card and foreground rack bars appearing blue and the detail behind the bottles progressively shifting towards red at the far distance.

    It is worth bearing in mind that by default the Viewer applies a range of depth color scheme and post-processing filter settings that are not present in a user-created script unless deliberately programmed in.  This is why Viewer images can look different to the output of scripts.

    It may be useful to refer to the information in the link below about configuring the color scheme in Python.

    https://github.com/IntelRealSense/librealsense/issues/7767#issuecomment-726704671

    0
    Comment actions Permalink
  • Yiherng

    Thanks for the reply, regardless of how I colorize the depth image, it seems like the stereo vision is susceptible to surfaces that have reflections ? Is there a way to reset and restart the camera besides unplug the camera ?

    0
    Comment actions Permalink
  • MartyG

    You can automatically reset the camera from a script using the hardware_reset() instruction.  It can be set up to trigger when certain logic conditions are met, such as more than 50% of the pixels having zero depth (indicating that something may have gone wrong with the image).

    The link below has an example of Python scripting for hardware_reset():

    https://github.com/IntelRealSense/librealsense/issues/3329#issuecomment-475293475

    I note in your Viewer image that you have two cameras.  If you have a multicam setup then more complex reset code would be needed that can check through all of the attached cameras.

    You can also reset manually from the RealSense Viewer by going to the More option near the top of the options side-panel and selecting the Hardware Reset option from its menu.  This has a similar reset effect to performing a camera unplug and replug..

    You can significantly reduce the negative effect of glare from reflections by adding a physical optical filter on the outside of the camera, over the top of the camera lenses.  The filter is called a linear polarization filter, and Section 4,4 of Intel's white-paper document about optical filters explains it. 

    https://dev.intelrealsense.com/docs/optical-filters-for-intel-realsense-depth-cameras-d400#section-4-the-use-of-optical-filters

    A 'without / with' image from the paper illustrating the glare negation that this filter can offer is below.

     

    0
    Comment actions Permalink
  • Yiherng

    So during the times when the depth readings were 0, I did try hardware_reset() to reset the camera, but the error "Frames did not arrive within 5000" popped up. I think it's because the device was reset yet wasn't ready to be turned on. I guess it needs device_hub to turn it on ? 

    I also tried to reset the USB port but it also didn't work. Here are the two functions I used to reset and restart the camera.

    def reset_device(query_serial_number):
     ctx = rs.context()
     device_list = ctx.query_devices()
     # print (device_list[0])
     for dev in device_list:
      if dev.get_info(rs.camera_info.serial_number) == query_serial_number:
      print("Found device, resetting")
      dev.hardware_reset()

    #################################################################################################

    def reset_usb():
     lsusb = Popen("lsusb | grep -i {}".format("Intel"), shell=True, bufsize=64, stdin=PIPE, stdout=PIPE,   close_fds=True).stdout.read().strip().split()
     decode_lsusb = []
     bus_number = []
     device_number = []
     for idx, x inenumerate(lsusb):
      # decode_lsusb.append(i.decode("utf-8"))
      if x.decode("utf-8") == 'Bus':
      bus_number.append(lsusb[idx+1].decode("utf-8"))
      if x.decode("utf-8") == "Device":
      device_number.append(lsusb[idx+1][:-1].decode("utf-8"))
     
    if len(device_number) == len(bus_number):
     for j inrange(len(device_number)):
      try:
       print("Opening", "/dev/bus/usb/{}/{}".format(bus_number[j], device_number[j]))
       f = open("/dev/bus/usb/{}/{}".format(bus_number[j], device_number[j]), 'w', os.O_WRONLY)
       fcntl.ioctl(f, 21780, 0)
      except:
       print("Failed to reset USB device")
    0
    Comment actions Permalink
  • MartyG

    If you have 2 cameras plugged in right now then I would suggest testing hardware_reset() with only one plugged in.  The simple version of the hardware_reset code will try to reset the first camera that it finds out of all those attached.  So I wonder if two cameras are attached, it might be trying to access the one that is not currently streaming and time-out (hence the 'within 5000' message).

    0
    Comment actions Permalink
  • Yiherng

    Okay I will try that. Thanks for your advice. Device class regardless in python or C++ should contain information particularly to one camera. If the camera has the correct serial number (like I did on my reset_device() function), it should not have problem to reset the device I ask. 

    If that's not the case, since the robot will have multiple cameras attached, I am wondering if there is a way to reset specific camera in multicam condition. 

    0
    Comment actions Permalink
  • MartyG

    I managed to locate the multicam reset script that I mentioned earlier.

    https://community.intel.com/t5/Items-with-no-label/D435-streams-work-once-then-crash/m-p/499732#M6053

    0
    Comment actions Permalink
  • Yiherng

    Thanks so much for your time, and I really appreciate your help on this matter. I will share my results for sure in the meantime, I hope you have a wonderful weekend. 

    0
    Comment actions Permalink

Please sign in to leave a comment.