View my account

RealSense D405 Class 1 Laser

Comments

2 comments

  • MartyG

    Hi Stan G Winston  The D405 camera model is not equipped with the Class 1 laser-based infrared projector that other 400 Series camera models (D415, D435, D435i, D435f, D455) have.

    0
    Comment actions Permalink
  • MartyG

    Mechanical drawings for the D401 camera module and Vision Processor D4 V4 board that are inside the D405 can be found on pages 133 and 135 of the current edition of the data sheet document for the 400 Series cameras.

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

     

    The chart below from the data sheet that compares which models of RealSense camera module are equipped with a projector (the Standard type or Wide type) also confirms that the D401 has neither type of projector.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.