RealSense D405 Class 1 Laser
Is the D405 a Class 1 laser device? All the documentation I can find shows the other D400 series cameras as Acitve IR and Class 1 laser - but not the D405.
The project I am working on does NOT allow class 1 laser devices. It looks like this camera will do the trick - but I need to certify that it isn't.
Thank you.
-
Hi Stan G Winston The D405 camera model is not equipped with the Class 1 laser-based infrared projector that other 400 Series camera models (D415, D435, D435i, D435f, D455) have.
-
Mechanical drawings for the D401 camera module and Vision Processor D4 V4 board that are inside the D405 can be found on pages 133 and 135 of the current edition of the data sheet document for the 400 Series cameras.
https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet
The chart below from the data sheet that compares which models of RealSense camera module are equipped with a projector (the Standard type or Wide type) also confirms that the D401 has neither type of projector.

Please sign in to leave a comment.
Comments
2 comments