Ron Vis
- Total activity 12
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 4
Posts
Recent activity by Ron Vis-
High-speed differential input signaling levels data sensitivity of D435 with USB2.0
Hello, What is the input signals leveling sensitivity (D+ D- ) of D435 for USB 2.0? For example - The USB standard defines -+175mV for far-end. Thank you,
-
No Frames received on D435 with USB2.1
Hello, I connect the D435 camera to PC with USB 3.2 ge1 and gen2 ports through USB 2.1 (because I can't work with USB3.2). I was unable to receive frames (white screen). After searching for some tr...
-
Intel realsense camera D400 series with Intel FPGAs
Hi, I'm trying to understand if I can do imaging processing on Intel's FPGAs connected to D400 series. And if it is possible, what should be the setup? is there an evaluation kit or project example...
-
Does D435i work with USB2.0?
Hello, I'm trying to connect my D435i to my PC (win10) using USB2.0 without success. Any suggestion? Thanks