Wafaa Mohamed

  • Total activity 4
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Wafaa Mohamed
  • Wafaa Mohamed commented,

    I tested the DHCP suggestion using both the locally built librealsense v2.58.2 tools and the system-installed tools, with the same result. rs-dds-config --dhcp on could not be applied because the c...

  • Wafaa Mohamed commented,

    No USB cable is connected to the camera. The camera is operating in Ethernet DDS mode only. The camera is connected through a TSW101 PoE switch. DDS discovery is working and the camera appears as: ...

  • Wafaa Mohamed commented,

    Thank you for the suggestion. Initially, I built librealsense v2.58.2 from source without explicitly enabling DDS support. After your recommendation, I rebuilt it with DDS enabled using: cmake .. \...