Sh Sh
- Total activity 4
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Sh Sh-
Sh Sh commented,
I confirmed Windows camera privacy settings are set to On but still same issue
-
Sh Sh commented,
I tried the camera only + usb with windows and i have tried to use linux windows and try to type ros2 topic list but the camera was not showing. Also I have tried to connect the camera through ethe...
-
Sh Sh created a post,
My D555 camera is working
I have bought 2 cameras of D555 and both of them are not working when connected in PoE. The LED lights of the ethernet port of the camera are not being turned on when the PoE is connected. Also i h...