Kevin Liao
- Total activity 11
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Posts
Recent activity by Kevin Liao-
[D457] Ma96712 + intel d457 in the Nvidia jetson platform
Hi I have an ODM project where the deserializer is a Max96712 connected to an Intel D457.I only see the source code for max9296 + max9295 in the master branch.May I ask if there is source code for ...
-
Realsense SDK can'work on the Nvidia Jetson Jetpack5.1.4 (linux kernel 5.10)
Hi RealSense TeamPreviously, when I followed the steps below to install SDK, I was able to use rs-capture to stream video from the D457 GMSL camera.However, last week, after installing the SDK usin...